Skip to main content
Zek_De
Senior
December 22, 2024
Solved

HSO Requirement for P-NUCLEO-IHM03 kit

  • December 22, 2024
  • 2 replies
  • 921 views

Hi everyone,
I am trying to activate HSO option for sensorless control which as much as I know this feature is to start motor without moving, but I cant activate HSO option with these option in attached.

Zek_De_0-1734882480515.pngZek_De_1-1734882494078.pngZek_De_2-1734882505570.pngZek_De_3-1734882528461.png

I cant find the problem. Thanks in advance.

Best answer by FouadB

Hello @Zek_De

As previously mentioned, if your goal is to generate a sensorless project with HSO enabled, we kindly recommend selecting the following:

Power board: STEVAL-LVLP01
Control board: B-G473E-ZEST1S

Best regards,
Fouad

2 replies

FouadB
ST Employee
January 2, 2025

Hello Zek_De,

Unfortunately, the P-NUCLEO-IHM03 kit is not compatible with the HSO option that requires phase voltage sensing.
You will need to use dedicated hardware boards: STEVAL-LVLP01 and B-G473-ZEST1S-B, which are supported in X-CUBE-MCSDK-6.
Please also refer to the HSO startup guide located in Documentation/HSO_Startup_Guide.pdf.

Best regards,

Fouad

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""
Zek_De
Zek_DeAuthor
Senior
January 2, 2025

according to workbench also I can use these, right?
EVALSTDRIVE101
NUCLEO-IHM09M2
B-G473E-ZEST1S
Because I can select these 3 in workbench application.

FouadB
FouadBBest answer
ST Employee
January 3, 2025

Hello @Zek_De

As previously mentioned, if your goal is to generate a sensorless project with HSO enabled, we kindly recommend selecting the following:

Power board: STEVAL-LVLP01
Control board: B-G473E-ZEST1S

Best regards,
Fouad

If you agree with my answer, please accept it by clicking on 'Accept as solution'.""