Question
I am using STM32H743VITx controller and i want to interface it with a BLDC motor.
While debugging the code everything works fine until i give command to start the motor i.e the moment i generate PWM and motor starts rotating, Cube IDE generates a message that the "target is not responding".
Also I've made sure that SWDIO, SWCLK, and SWO pins are correctly mapped on the controller.