Skip to main content
SBrah.1
Visitor II
January 27, 2023
Question

I am Using X-nucleo-ihm07m1 along with nucleo-f030r8 for controlling a bldc motor. once my motor enters in FOC Mode it shows over current error. what Could be a possible reason? What Can I Try

  • January 27, 2023
  • 2 replies
  • 1480 views

..

This topic has been closed for replies.

2 replies

Cristiana SCARAMEL
Technical Moderator
January 31, 2023

Hello @SBrah.1​ and welcome to the ST Community.

Are you using the STM32 Motor Control Software Development Kit X-CUBE-MCSDK?

If so, what version?

Could you share more details on your application?

  • Single o three-shunt configuration
  • Sensored (Hall or encoder feedback) or sensorless (BEMF detection)

According to these hardware and firmware settings you can check the OC threshold set and verify if the over current protection is properly triggered by application.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Associate II
February 8, 2024

i have the same problem while using single shunt (sensorless) , motor pilot didn't even connect to the board

ABart.5
Associate II
April 26, 2023

Were you able to figure out the problem? I'm having the same issue.