Question
I can't complete ST Motor Profiling
- April 3, 2024
- 2 replies
- 2597 views
Hello,
Hardware : NUCLEO-G474RE + X-NUCLEO-IHM08M1 + DollaTek 2204 BLDC motor
Software : Motor Control Benchwork 6.2.1, STM32CubeIDE 1.13.1
When I try to start motor profiling the motor starts to produce radom beeps, vibrations and accidental spins. The profiling reaches 28% and then the motor stays in that state forever. What can I change to make the motor rotate correctly and to finish profiling successfully?