Skip to main content
Associate III
February 7, 2026
Question

Imax Setting for 2928.86 gf·cm Torque Operation

  • February 7, 2026
  • 1 reply
  • 152 views

I would like to ask for your guidance regarding the motor current setting under a specific torque condition.

Based on the motor datasheet,

pelino_0-1770472140317.png

I derived a linear torque–speed relationship and confirmed that, at a torque of 2928.86 gf·cm,

the motor is expected to operate at 444 rpm, requiring approximately 6.6784 A according to the calculation.

The assumptions and parameters used are as follows:

  • No-load speed: 5000 rpm

  • Rated speed: 4000 rpm

  • Rated torque: 0.063 Nm (642.86 gf·cm)

The derived relationship is:
n = A × T + B
where
A = −1.55556, B = 5000

At the target speed of 444 rpm, the estimated torque is:
2928.86 gf·cm

The required current was estimated using the torque constant calculated from the rated condition:

  • Rated current: 1.7 A

  • No-load current (I₀): 0.3 A

Kt = 642.86 / (1.7 − 0.3) = 459.184 gf·cm/A

Using this value, the estimated current is:
I = (2928.86 / 459.184) + 0.3 ≈ 6.6784 A

However, when measuring the same motor using ST Profiler to obtain the Electrical Model and Mechanical Model, the result showed Imax = 1.38 Apk.

pelino_1-1770472194019.png

Please note that:

  • The actual motor drive board is EVSPIN32G4-DUAL.

  • ST Profiler does not support EVSPIN32G4-DUAL, so the Electrical and Mechanical Models were measured using X-NUCLEO-IHM16M1 instead.

Based on this, I would like to ask whether it is acceptable to set Max current to approximately 7 Apk in order to achieve 2928.86 gf·cm torque with this motor, or if there are any limitations or concerns from the motor or driver perspective.

pelino_2-1770472744539.png

 

 

Your advice would be greatly appreciated.

Best regards,
Pelino

1 reply

GMA
Technical Moderator
February 23, 2026

Hello @pelino,

The profiled maximum current (Imax) is 1.38 A. Why is 0.15 A mentioned on the WB interface?
The BL42S-24026N (26 W) motor documentation specifies a rated current of less than 1.7 A and a power rating of 26 W. Exceeding these values is not recommended.
The motor documentation also provides a torque table:

image.png

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA