Inertia and cut-off frequency parametrs in Motor SDK 5.Y.3 for E-Scooter application
I am trying to find the correct PI controllers parameters for my E-Scooter application. Initially, I determined the parameters of the motor through the Motor Profiler, but now I wondered what inertia should be specified. The inertia of the engine idle is quite small, but when the E-Scooter moves with a passenger, the inertia of such a system is many times greater. Since the calculation of PI controllers depends on this, I would like to better understand how I should calculate it. I am also interested in the cut-off frequency parameter, since I have a low-speed application of only 500-600 rpm max, which frequency should I set if I do not need high-frequency pulsations that may arise during control.