Skip to main content
KStew.1
Associate II
March 18, 2025
Question

ioc file not generated from Motor Control Workbench - template inclusion failed

  • March 18, 2025
  • 2 replies
  • 599 views

Using Version: 6.3.2

I have a custom motor and a custom inverter board, importing these works fine in my project but when I try to generate the project I get the following:

2025-03-17 17:54:58,571 ERROR [LineInfo_to_exitCode.manage_IocGenerationError] Unable to generate ioc file due to: Template inclusion failed (for parameter value "STM32F769NI/STM32F769NI - 216 MHz - int.ftl"):...

I tried changing the MCU on my inverter to see if this was specific to a board and I keep getting the same bug. Please help :)

 

2 replies

GMA
Technical Moderator
March 18, 2025

Hello @KStew.1,

Supported mcu are located on "MC_SDKToolDirectory\Utilities\PC_Software\STMCWB\assets\hardware\mcu" directory.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
KStew.1
KStew.1Author
Associate II
March 31, 2025

The STM32F769NIHx JSON file is in that folder, this issue persists

GMA
Technical Moderator
April 1, 2025

Hello @KStew.1,

Can you share your custom board .json file and your associated .stwb6 file?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA