Question
IPM30B: minimal working setup
Hello,
Is there any resource or reference available like tutorial video or presentations to set up a minimal working configuration for the IPM30B? I have experience on a low power setup with X-NUCLEO-IHM16M1 but I am new to hardware assemblying with ST and I am trying to understand how to correctly configure a basic setup to make the motor start. My goal is to have a minimal working system, including:
- IPM30B power stage
- G431RB or G474RE development board, with the suitable motor control connector and with flat cable
- Two separate low voltage DC supplies (one for auxilliary 15V port and the other one for Vdc bus)
- Low power PMSM with 24V nominal voltage
- Basic configuration using Motor Control Workbench / MCSDK for PMSM sensorless basic operation
At the moment, I am not sure about the correct jumper connections required to match the configuration settings in ST Motor Control Workbench, the proper wiring details between the IPM30B and the control board, and the correct procedure to safely power on the setup. I am also looking for any reference design, example project, or application note that could be used as a starting point. I have correctly placed the C1 capacitor.
Any guidance, documentation, or example would be highly appreciated. Thank you in advance.