is it possible to run over 40000RPM with 8 poles motor on STSPIN32F0
I use 16KHz PWM to run motor, once the motor over 24000RPM, the motor current will become very high and unstable. it is seems over than FOC execute rate cause this problem.
I'm not sure I think is right or not ? is there any suggestion please tell me.
when I use G431B MCU with 30KHz PWM to run same motor, it looks run very well with no problem (can over 40000RPM)
P.S
1. motor parameters: Vm: 12v / Rs: 0.3 ohm / Ls: 20uH