Issues with 2 Motor Configuration and Current Sensing in MC Workbench for Customized Controller Boar
- June 20, 2024
- 2 replies
- 1850 views
Hello STM32 Community,
I am currently working on a customized controller board with the same architecture as the EVSPIN32G4-dual, using the STSPIN32G4 and STDrive101, to control two BLDC motors. However, I have encountered a few issues and would appreciate any guidance or confirmation on the following points:
2 Motor Configuration with 6-Step Algorithm: While setting up the MC Workbench, I noticed that I cannot select a 2 motor configuration when I choose the 6-step algorithm. Although I believe this might not be a significant issue, I would like to confirm if it is still possible to configure the PWM peripheral for the second motor manually? Any advice or steps to achieve this would be highly beneficial.
Current Sensing with 6-Step Algorithm: Additionally, I found that the current sensing section is disabled in the MC Workbench when using the 6-step algorithm. I am interested in acquiring current readings with a single shunt configuration. Is there any possibility to enable or implement current sensing in this scenario, even though the MC Workbench doesn't provide direct support for it?
Thank you in advance for your assistance!
Best regards,