L6470 Run command (relation among MAX_SPPED, MIN_SPPED and SPD values)
Hi, I'd like to use Run command for my stepper motor as follows. How can I set values in registers?
- Maximum speed: 4000step/s
- Minimum speed: 500step/s
- SPD: 1000step/s
According to the data sheet, I can calculate the values for MAX_SPEED, MIN_SPPED and SPD in (Run command) as follows.
- MAX_SPEED: 4000 x tick / 2^(-18) =4000 x 250 x 10^(-9) / 2^(-18) = 262
- MIN_SPPED: 500 x tick / 2^(-24) = 500 x 250 x 10^(-9) / 2^(-24) = 2087
- SPD: 1000 x tick / 2^(-28) = 1000 x 250 x 10^(-9) / 2^(-28) = 67108
In the data sheet, Run command has Note section. According to the statement, MIN_SPPED <= SPD <= MAX_SPPED but my calculated values are MAX_SPEED < MIN_SPEED < SPD. Even though these settings, does motor rotate correctly?
Note: The SPD value should be lower than MAX_SPEED and greater than MIN_SPEED otherwise the Run command is executed at MAX_SPEED or MIN_SPEED respectively.
https://www.st.com/ja/motor-drivers/l6470.html