Skip to main content
tmaun.1
Associate II
February 13, 2023
Question

Launch a function automatically when program stops at a breakpoint

  • February 13, 2023
  • 8 replies
  • 3199 views

Hi, I would like to launch a function automatically when my program stops after a breakpoint.

I work on motor control application and it is recommanded to disable PWM channel before a breakpoint.

How I do configure cubeide ? thanks for your help

This topic has been closed for replies.

8 replies

Fred V.
ST Employee
February 20, 2023

Hello,

If you are using an Advanced Timer to generate the PWM channels, you benefit from its Debug mode. On a breakpoint, the timer can be configured to either stop counting or carry on counting. This is configured in the debug module. On STM32G4xx and STM32F3xx MCUs, if the timer counter is stopped on a breakpoint, its output is disabled.

So, there is no need to ask STM32CubeIDE to disable the PWM output on a break point, this can be done directly by the MCU itself.

Now, breaking the software while the motor is controlled can be dangerous as it may result in high currents that may destroy the boards and/or the motor. If you really need to do so, it is strongly recommended to set a maximum current limit on your power supply.

Best Regards,

Fred.

tmaun.1
tmaun.1Author
Associate II
February 21, 2023

Hello,

Thank you for your reply. Indeed, it is not recommended to place breakpoints while the motor is running. But sometimes, it happens forget a breakpoint, do a bad manipulation or a bug and the program can stop while the engine is running. On certain IDEs like those of RENESAS, for example, you can configure the debugger to launch a function (written by the programmer who codes what he wants in his function, even the launch of a measurement) automatically after stopping the program whatever the event (breakpoint, Stop, Pause, bug etc...), Is CUbeIDE able to do it ? because it is a very robust debugging option to avoid breaking MOS. THANKS

Fred V.
ST Employee
February 21, 2023

Hello,

What about using the Debug mode of the Advanced Timer as proposed in my previous answer? If you use either a G4 or an F3, it would do the same as what the debugger would do. Now, if you really need to do this through the debugger, I cannot help you there. I'll let others provide the information.

Best Regards,

Fred

waclawek.jan
Super User
February 21, 2023

Hi @Fred V.​ ,

Are you talking about this:

For safety purposes, when the counter is stopped (DBG_TIMx_STOP = 1), the outputs are

disabled (as if the MOE bit was reset). The outputs can either be forced to an inactive state

(OSSI bit = 1), or have their control taken over by the GPIO controller (OSSI bit = 0) to force

them to Hi-Z.

?

Is this only in the 'F3 and 'G4 mcus?

Is this only in the Advanced Timers (TIM1, TIM8, TIM20)?

I'd recommend to add this to the overall block schematics of these timers, it may be quite surprising to the unaware.

JW

Tesla DeLorean
Guru
February 21, 2023

This "call on breakpoint" methodology isn't particularly prevalent.

Generally there are a lot of systems where dead-stopping like this can be catastrophic.

Here its perhaps best to instrument, and have an emergency stop button via a high priority EXTI, or wrapping breakpoints in a routine that gets the system into a safe/safer state before trapping to the debugger.

Also wrap any hard fault or error handlers so they fail safe too.

Output trace, diagnostic and telemetry so behaviour can be characterized.

TBH understanding program logic and flow should be done earlier.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Fred V.
ST Employee
February 21, 2023

Hi @waclawek.jan,

I am indeed talking about this. The Debug Mode seems to exist on all timers (usually described the last sub-section of the functional description of the timer. However, the safety behavior you mention is not. You can find it on Advanced Timers, HR Timers and some GP Timers of the STM32F3, F7, G0, G4 and H7. It is not present on F0 and F4. I did not check the other series.

BR

Fred

waclawek.jan
Super User
February 21, 2023

Thanks, @Fred V.​ .

> It is not present on F0 and F4

Indeed, RM0091 for 'F0 does not mention it, but:

0693W00000aHKszQAG.pngI guess you've checked some other 'F4 then the "classics" covered by RM0090, in which case determining whether this feature is or is not present may be more tricky than I thought...

JW

Fred V.
ST Employee
February 22, 2023

Yes, you're right. I overlooked RM0090 and only looked at RM0390 which describes STM32F446xx devices. Sorry. Indeed, I do not see any easy rule to determine whether the feature is present on a given MCU.

Fred.

KnarfB
Super User
February 22, 2023

Back to the original question: ".. would like to launch a function automatically when my program stops after a breakpoint"

Yes, that can be done with STM32CubeIDE's debugger gdb. The Debugger Console View in STM32CubeIDE is needed to enter interactive commands.

Prepare a C function that should be called, for testing I used blink() which blinks a LED few times.

Make sure that the function is not optimized out by the complier/linker, e.g. by calling it once in the code or some tool magic.

Start debugging, set a breakpoint and stop at it. Debugger Console output like:

Temporary breakpoint 2, main () at ../Core/Src/main.c:78
78	 HAL_Init();
 
Breakpoint 1, main () at ../Core/Src/main.c:104
104		 printf("Hello\n");

enter:

commands 1 
> call blink()
> end

next time you stop at breakpoint 1, the function will be called.

Notes:

  • call can be used directly to execute some fct. out of context
  • more/other commands are possible to register

get more help from the Debugger Console:

help commands
help commands
Set commands to be executed when the given breakpoints are hit.
Give a space-separated breakpoint list as argument after "commands".
A list element can be a breakpoint number (e.g. `5') or a range of numbers
(e.g. `5-7').
With no argument, the targeted breakpoint is the last one set.
The commands themselves follow starting on the next line.
Type a line containing "end" to indicate the end of them.
Give "silent" as the first line to make the breakpoint silent;
then no output is printed when it is hit, except what the commands print.
help call
Call a function in the program.
Usage: call EXP
The argument is the function name and arguments, in the notation of the
current working language. The result is printed and saved in the value
history, if it is not void.

hth

KnarfB

tmaun.1
tmaun.1Author
Associate II
February 22, 2023
Thanks KnarfB for your answer ! it is working. We have to do that for each new breakpoint we add ?
It is shame that is more complicated than Renesas IDE ( as E2studio or HEW) where we can define the function which is calling when the program stops for any reason.
KnarfB
Super User
February 22, 2023
waclawek.jan
Super User
February 22, 2023

@KnarfB​ ,

nice, thanks!

Jan