libImpedCorr.a fail
Hi, Dear STM experts:
I used MCSDK6.3.2 HSO for BLDC control when porting from stm32Q473 to stm32f405, but when using void IMPEDCORR_setLs_si(IMPEDCORR_Handle pHandle, const float_t Ls_H); A hardware failure occurred during the function, and the possibility of external parameter input has been ruled out. Therefore, I would like to confirm again that the libImpedCorr. a library file must rely on the stm32Q47x chip to run?If necessary, then I can only give up the transplant.Hope to receive a reply。
Best Regards.