Skip to main content
fDUMA.1
Associate
September 30, 2022
Question

Link to download STSW-SPIN3204 firmware package?

  • September 30, 2022
  • 2 replies
  • 886 views

..

This topic has been closed for replies.

2 replies

Cristiana SCARAMEL
Technical Moderator
September 30, 2022

Hello @fDUMA.1​ and welcome to the ST Community.

You can find the firmware package for the STEVAL-SPIN3204 board in the STM32 Motor Control SDK (X-CUBE-MCSDK-Y)

"If you feel a post has answered your question, please click ""Accept as Solution"""
fDUMA.1
fDUMA.1Author
Associate
September 30, 2022

BIG BIG BIG problem to make this card (STEVAL-SPIN3204) work!! 3 days I'm trying to use it !!!

The challenge is to find the good programs. ST documentation is SO bad!

Ok I've installed X-CUBE-MC SDK - Y

(the note UM2310 is note usefull - lost time to seach this firmware which does not exist anymore!!)

Anyway... I try to use the example 6S_STEVAL_SL_VM

In ST Motor Control Workbench, at the top of the page it is written "Control Board STEVAL_SPIN3201"... I hope it's a mistake besause it is the example for my board SPIN3204...

I compile...

I open the project in STM32cubeIDE (What a headache for a rooky to make the difference beetween STM32cubeMX and STM32cubeIDE - How many soft to use a ST microcontroller??) When you used to use an Arduino or a PIC, it's so diferent, it is not understandable!!

A general presentation of how we must do to use your products is missing.

Anyway... I compile the project in STM32cudeIDE and I click on "run" to program the microcontroler on the board (SPIN3204)

I return to ST MC workench (ver 5.Y.4), and I click on "motor Pilot"

When I click on "connect" I obtain this answer:

0693W00000UFXFYQA5.pngIt is written "try to configure the board", and in the application, all is grey, I can't use it.

In the terminal windows, I have this:

0693W00000UFXK4QAP.pngWhat must I do??

Can you help me please?

Fabrice