Skip to main content
Associate
February 5, 2025
Solved

MC Workbench 6.3.2 B-G431B-ESC1

  • February 5, 2025
  • 1 reply
  • 1098 views

Hi everyone,

I'm working with the B-G431B-ESC1 board and need help setting up overcurrent protection. I want to ensure safe operation and prevent damage to the hardware.

Could anyone guide me on the best way to configure the current sensing and protection in MC Workbench?

Any insights, step-by-step instructions, or shared experiences would be greatly appreciated!

Thanks in advance! :rocket:

LSerhii_0-1738769957414.pngLSerhii_1-1738770007818.png

 

Best answer by Gael A

Hello LSerhii,

For some reason your B-G431-ESC1 description does not feature the OCP. Please make sure that you are up to date with our latest MCSDK version (6.3.2) and then recreate a project from scratch while making sure you are using the board description provided inside the package.
There should be no reason for your project not to feature the OCP.

1 reply

Gael A
Gael ABest answer
ST Employee
February 5, 2025

Hello LSerhii,

For some reason your B-G431-ESC1 description does not feature the OCP. Please make sure that you are up to date with our latest MCSDK version (6.3.2) and then recreate a project from scratch while making sure you are using the board description provided inside the package.
There should be no reason for your project not to feature the OCP.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
LSerhiiAuthor
Associate
February 6, 2025

Hello Gaël A.

I think there is an issue with this version (6.3.2). I am consistently getting the OCP error.
Could you confirm it ?

LSerhii_0-1738864355670.png