MC Workbench change mcu analog voltage reference
I am working working with a PMSM FOC project in MC Workbench 6.2.1 and I am wondering if there is a way to change the mcu's analog vref input voltage. From the numbers I'm seeing on the current measurement page, it seems like MC Workbench is expecting the mcu to have a 3.3v reference on the vref input pin of the mcu. However, I don't see a way to change that in MC Workbench or a field for it in any of the board files for the control or power boards. The custom board I am using has a 3.0v input to the vref+ pin on the mcu. Is it possible to input this information anywhere?