MC Workbench GENERATION reports errors for any of the included example projects.
Help! I'm new to ST development tools. All I'm trying to do right now is generate an MC Workbench example project. Any example project.
MC Workbench GENERATION always reports the following error:
"The ST intranet updater server is unknown: mcucrossselector.codex.cro.st.com"
Any suggestions greatly appreciated.
-----
Details:
MotorControl Workbench 5.Y.4 (en.X-CUBE-MCSDK_5.Y.4_v5.5.4.zip)
STM32CubeMX 6.4.0 (en.stm32cubemx-win_v6.4.0.zip)
STM32CubeIDE 1.7.0 (st-stm32cubeide_1.7.0_10852_20210715_0634_x86_64.exe)
(All downloaded and installed yesterday.)
It does generate a CubeMX project, which generates a CubeIDE project, but that source code is has a massive number of undefined symbols. I have not changed any config or preferences settings. It's all "fresh out of the box", and I'm just following the provided instructions.
((Context: I have 2 new B-G431B-ESC1 boards, and started out trying to build the example projects for that board. When that failed, I started trying other examples, and it looks like the problem is a very basic one with MC Workbench, not related to the examples for my specific board.))