Skip to main content
Associate
August 27, 2024
Solved

MC Workbench Phase Voltage Sensing

  • August 27, 2024
  • 2 replies
  • 1270 views

Hello,
I am designing FOC motor controller based on DRV8316. For this, I am adding a DRV8316 custom board in the MC Workbench. Please find the JSON file attached. 
The problem is that I am unable to add phase voltage sensing. Although I have added phase voltage sensing in the JSON file it is not appearing in MC Workbench.

Thanks

 

farzansaleem_0-1724785407643.png

farzansaleem_1-1724785424396.png

farzansaleem_2-1724785589618.png

 

 

    Best answer by Gael A

    Hello farzansaleem,

    Unfortunately, Phase Voltage sensing is currently only supported by HSO and ZeST algorithms, which are not supported on STM32H5.
    All information concerning those two algorithms can be found on our STM32 ZeST page.

    2 replies

    August 28, 2024

    Hey @farzansaleem 

    I highly recommend you to use the MCSDK V6.3

    It is so much easier for implementing a custom board.

    Regards

    Associate
    August 28, 2024

    Thanks for the recommendation. I have tried MCSDK V6.3, yes it is easy to implemet custom board in it. But phase voltage sensing is also not working in MCSDK V6.3.

    Gael A
    Gael ABest answer
    ST Employee
    August 28, 2024

    Hello farzansaleem,

    Unfortunately, Phase Voltage sensing is currently only supported by HSO and ZeST algorithms, which are not supported on STM32H5.
    All information concerning those two algorithms can be found on our STM32 ZeST page.

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.