MCSDK 6.2.0 is out!
Dear MCSDK users, MCSDK version 6.2 is now available: Download It here.
Here are the main changes for this version:
Hardware Compatibility :
- C0 Support for FOC 3-Shunt and 6 steps
- H5 Support for FOC 3-Shunt and 1-Shunt
- Add support of All MCUs part number of F3,G4,G0 series
Motor Control Features:
- Support of dual drive for F3,F4,G4
- Addition of ICS (Insulated current sensor)
Tools:
- Improve user guidance with accurate inline documentation about the board's modifications
- Improve user flow with IOC reading capability
- The user is now able to generate his own profiler firmware with the desired combination of Boards from the Workbench. You can find the details in the profiler documentation available in the user manual.
We also introduced new boards like: EVLSPIN32G4-ACT, EVSPIN32G4-DUAL, NUCLEO-C031C6, NUCLEO-H563ZI, NUCLEO-H503RB, B-G473E-ZEST1S-B, STEVAL-LVLP01
The boards here below, already supported in MCSDK 5.4.8, are now supported in MCSDK 6.2.0: STEVAL-IHM039V1, STEVAL-IHM045V1, STEVAL-CTM009V1, STEVAL-IHM042V1, STM32L476G-EVAL, STM32F769I-EVAL
Do not hesitate to respond under this post to give us your opinion about this new version.
Best regards