MCSDK 6 board config
Using the SDK I am basing a new system on the EVSPIN32G4. After selecting the inverter, and motor, I am then taken into the parameter configuration of the motor driver.
According to the boards manager the EVSPIN32G4 has multiple configurations available for single ended and differential current shunt configurations, plus using 3 op-amps, one for each current shunt etc, for the most system flexibility. Yet in the parameter configuration section of the SDK, when selecting this board, you have no control over the configuration of the current shunts and are locked into a single ended, triple shunt, system using only two op-amps. You can select to use either internal (PGA), or external resistor configurations but that's it. Moreover a triple shunt, triple op-amp, with external resistors, is the default hardware configuration for this board, so selecting something other than this (such as using the PGAs) should require hardware modifications but the SDK doesn't think this is necessary.
This doesn't seem to make any sense.
Additionally, with sensor-less control, the MCU should require voltage feedback from the three driven phases. These are already a part of the base hardware configuration for the EVSPIN32G4 board but there's no mention of this requirement, or input pin configuration, within the SDK.
Is there something I am doing wrong here to enable the configuration of additional parameters?
Many thanks,
Matt.