Solved
MCSDK generation error : Error = zip END header not found
- May 23, 2025
- 1 reply
- 515 views
Hello,
There is a error during code generation phase on MCSDK.
2025-05-23 19:02:39,600 ERROR [LineInfo_to_exitCode.log_LineInfo] Error = zip END header not found
2025-05-23 19:02:39,601 WARN [LineInfo_to_exitCode.log_LineInfo] Failed to launch self-upgrade
But, click RUN CUBEMX button, the tool can be opened and generate code that can be compiled successed on IAR.
Will that error have a negative impact on the program?
the attachment files include : 3 pictures of configure and generation.