MCSDK motor startup short circuit
Hello,
when referencing a position control with a new custom hardware, there is a short circuit of the power supply at the beginning of the referencing. The STM32 G4 with the MCSDK 5.4.8 is used. The setup already ran on a first own board so that the parameters worked so far. Only a new gate driver with integrated current amplifier was used. The assumption is a faulty current amplification. The TI DRV8304H is used and the circuit is designed regarding to the reference design. Is the internal amplifier circuit compatible with the MCSDK at all?
If there is any experience, I would be very pleased about. Thanks