Skip to main content
JPate.7
Visitor II
July 11, 2024
Question

Measure Individual Phase Current

  • July 11, 2024
  • 1 reply
  • 590 views

hello sir

I am using motor control workbench 5.4.6 and EVSPIN32F0602S3 kit. Is there any function to get individual phase ( R,Y,B) current and total average power of motor ?

    1 reply

    Cristiana SCARAMEL
    Technical Moderator
    August 6, 2024

    Hello @JPate.7 

    I suggest to download the new version of STM32 Motor Control SDK (X-CUBE-MCSDK6)

    In the "Motor Pilot" --> tab "Registers" you have access to all variables: you can read or plot them.

    The current phase are I_A e I_B (the I_C can be obtained because the sum of all three is zero) the MOTOR_POWER is the total power of motor.

    "If you feel a post has answered your question, please click ""Accept as Solution"""