Skip to main content
Associate
June 30, 2025
Solved

Motor control SDK - manual control API implementation

  • June 30, 2025
  • 2 replies
  • 546 views

Hi all,

I am using the STSPIN32G0252Q chip on a custom board (implements 3-shunt current sensing and back-EMF measurement, alongside the required drive features). I have designed the board in the MC Workbench, and have manually profiled the motor I am using, as the motor pilot tool doesn't support the Cortex-M0+ range.

However I am finding it difficult to know where to start with actually implementing the code generated by the workbench/CubeMX; I can see that all of the control functionality is present, but there doesn't seem to be any documentation on how to actually run a motor using just API/HAL calls, instead of using the motor pilot. I have read the SDK documentation, but while this lists all of the functions and control algorithms it doesn't seem to show what a simple implementation loop would look like. Worse still, there seems to be some conflicting information about what each function does (e.g., whether the MC_StartMotor function needs a speed/torque ramp pre-programmed or not).

Does anyone have any tips to point me in the right direction?

Thanks in advance!

Best answer by Gael A

Hello DMorris42,

Could you please tell me which version of the MCSDK you are using ?

Also, I would like to know where the conflicting information is located in the documentation, as I can't seem to find the one you are referring to : 

bool MC_StartMotor1 (void)
 Initiates the start-up procedure for Motor 1.

Extract from MCSDK documentation.

The start-up ramp is already computed by the WB given your system's characteristics, but you can change it in WB or after generation in drive_parameters.h or directly in the RevUpControlM1 handler in mc_config.c.

2 replies

Senior III
June 30, 2025

mc_api.c contains all the functions to run the motor in different modes and stop motor, this file is sufficient to drive the motor.

Gael A
Gael ABest answer
ST Employee
June 30, 2025

Hello DMorris42,

Could you please tell me which version of the MCSDK you are using ?

Also, I would like to know where the conflicting information is located in the documentation, as I can't seem to find the one you are referring to : 

bool MC_StartMotor1 (void)
 Initiates the start-up procedure for Motor 1.

Extract from MCSDK documentation.

The start-up ramp is already computed by the WB given your system's characteristics, but you can change it in WB or after generation in drive_parameters.h or directly in the RevUpControlM1 handler in mc_config.c.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.
DMorris42Author
Associate
June 30, 2025

Hi Gael,

I'm using SDK version 6.4.0.

Ah right, it wasn't clear to me that the startup ramp from the WB was pre-programmed for the motor - from reading the documentation it seemed that this needed to be programmed every time, which I found conflicted with the wiki:

https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_Motor_Control

as this doesn't discuss control profile generation.

Thanks for the input!