Motor Control using Nucleo-G071RB+IHM16M1
Hello ST Community
I am experiencing issues while trying to operate the GBM2804H-100T Motor with the nucleo G071RB board and IHM16M1 motor driver board.
The G431RB board and IHM16M1 motor driver board are succeeded in operating the motor. But in the case of the nucleo G071RB board and IHM16M1 motor driver board are some error occured for example,can't connect to motor pilot GUI and also FOC duration error in the GUI.
■Our Developement emvironment
・Software:Generated by MCSDK6.3.0/STM32 Cube MX
・Compiler:STM32CubeIDE 1.13.2
・ST Motor Pilot V1.2.9
what will be the issue , can anyone help me with this.