Motor profiler bugs
Hello,
I'm playing with a nucleo-F446 + IHM16M1.
The MC workbench is able to generate code. I am able to compile and program it using cube IDE. Running the default Gimbal motor with the standard parameters is still painfull. I'm trying to get a better motor profile with the profiler tool.
Using MC workbench 6.1.0, the motor profiler tool can't be run :
- Discover board returns "This MCU is not supported"
- Manually selecting the board show an empty screen (no board listed)
After an update to v6.1.2, things are better but still not working:
- Discover board returns "failed to discover board"
- Manually selecting the board show the complete list. After selecting my HW config, I have a pop-op requesting a FW update. This update don't works, the software returns back to the board list screen without showing any error.
In the terminal, many errors are shown (ERROR:ASPEP BEACON TIMEOUT 500ms).
Any ideas will help
Thanks