Motor Profiler connection error: Port Open and try to configure the board
I'm using the Nucleo-F302R8 and the X-Nucleo-IHM07M1 with the small kit motor it comes with. I'm having trouble getting the motor profiler to connect to the board.
The F302R8 seems to have the demo motion program running, since I can hit the blue button to start the motor turning. But if I want to run the profiler windows application and try to connect to the board, I get this error:
"Port Open and try to configure the board"

I've tried updating STLink, and it's on the latest (v2.j37.m26). I've updated my USB driver. I can connect to the board using ST-Link Utility. But the motor profiler can't connect.

What might be preventing motor profiler from connecting?