Motor Profiler connection issue, Motor Pilot works fine
I can use the Motor Pilot ok but when I try to connect with the motor profiler I see a momentary connection when left in "polling" mode where the B-G431B-ESC1 board flashes on screen, then the board disconnects and the image disappears. Here's the logs:
[INFO] - : Connecting to Board
[INFO] - UART worker: Successfully open port COM3 @ 115200
[INFO] - : try to configure the board
[INFO] - : Connected to board
[INFO] - : Disconnected from boardWhen I try to connect in non-polling mode I stay connected but no board appears and all the buttons are grayed out.
Just now I confirmed that the Motor Pilot is working again. Then I disconnected with Pilot and reconnected with the Profiler. Now the Profiler program allows me to click on "Start Profile" but that results in an error below:
[INFO] - : Application is starting : MotorPilot version:1.2.5
[INFO] - : ini file path=C:/Users/COSMED USER/AppData/Roaming/ST Microelectronics/ST Motor Pilot.ini
[INFO] - : Polling time out is set to 200 ms
[INFO] - : set qml to : qrc:/GUI/MC_FOC_SDK.qml
[INFO] - : sdkPath=C:/ST/MC_SDK_6.2.1
[INFO] - : Loading registers bank desciption file C:/ST/MC_SDK_6.2.1/Utilities/PC_Software/STMotorPilot/RegisterList/RegListProfiler_MCPV2.json
[INFO] - : Registers bank description loaded successfully
[INFO] - : Load Application qrc:/GUI/profiler.qml
[INFO] - : QML Application ready
[INFO] - : Connecting to Board
[INFO] - UART worker: Successfully open port COM3 @ 115200
[INFO] - : try to configure the board
[INFO] - : Connected to board
[ERROR] - MotorControlProtocol: ASPEP_RESP ERROR:CMD_UNKNOWN
MCW 6.2.1
Motor Pilot 1.2.5
I also tried:
MCW 6.2.0
MCW 6.1.0