Skip to main content
GJamo.1
Associate II
June 8, 2023
Solved

Motor profiler restrictions

  • June 8, 2023
  • 2 replies
  • 1152 views

I'm using motor profiler for the motor control. I have the following hardware components:

  • STM32 Nucleo-F4446RE
  • X-NUCLEO-IHM16M1
  • Mitoot motor

In the motor profiler, it mentions that IHM16M1 can only work sith STM32 Nucleo-G4 and that F4 and IHM16 combined is not supported.

Is there a workaround available to test the motor despite this limitation?"

This topic has been closed for replies.
Best answer by cedric H

Hello @GJamo.1​,

Which version of the MCSDK do you use?

I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.

Regards

Cedric

2 replies

cedric H
cedric HBest answer
Technical Moderator
June 8, 2023

Hello @GJamo.1​,

Which version of the MCSDK do you use?

I just checked with the MCSDK 6.1.2, and the combinaison Nucleo-F4446RE+X-NUCLEO-IHM16M1 is proposed by the profiler.

Regards

Cedric

GJamo.1
GJamo.1Author
Associate II
June 8, 2023

Thanks for the info