Question
Motor Profiler with STM32303E-EVAL + STEVAL-IPM15B 3Sh
Hi Expert,
I wan to use STM32303E-EVAL + STEVAL-IPM15B 3Sh to run the motor profiler 5.4.8.
But the error message is shown below.
I connect the control board to PC via USB, the LD8 is red. The device manager of PC cannot see com port.
I think the STM32303E-EVAL not provide a virtual com port, right?
How could I solve this problem?
Thanks.