Motor's current & speed overshoot when load is released
Hey,
So we're trying to modify the motor control SDK to fit our needs.
We currently use the EVSPIN32G4 to evaluate the performance of the motor control SDK with our motor and our requirements.
We're using an SM-PMSM motor, which works in a rated voltage of 24V, max current of 24A and 21 pole-pairs and has Hall sensors installed. We're trying to spin it using Hall sensored-FOC.
The issue we're facing, is that when we release an applied load on the motor at once, the motor's speed rises significantly, followed by a big spike in the current in-take of the motor.
It often leads to over-current or over/under voltage faults.
Is there a way to control that big spike?
Thanks,
Eyal