Skip to main content
Associate II
May 20, 2025
Question

Motor startup failure error

  • May 20, 2025
  • 1 reply
  • 790 views

Dear Support team,

I am currently working on a sensorless motor control application using the Observer + PLL algorithm to run a 24V PMSM motor (rated at 3600 RPM, no load) on a custom driver board based on the STM32F030R8. My PWM frequency is 8000kHz and I am using a single shunt resistor for current sensing.

The motor appears to operate correctly during the ramp-up phase. However, it stops immediately after transitioning to closed-loop FOC, triggering a startup failure error.

I am using STM32 Motor Control Workbench version 5.4.8 for configuration. I have attached the wb file and .stmcx file in .txt format containing the full GUI-based configurations for your reference.

I would appreciate your assistance in resolving this issue.

1 reply

Associate II
May 20, 2025
GMA
Technical Moderator
May 20, 2025

Hello @Abhishek_n17,

Refer to our FAQ Wiki page available here, Chapter 2.11 / 2.12 about Startup failure error.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
Associate II
May 21, 2025

Thanks for the reply. I have tried all possible combinations from the link you have mentioned, but my motor still is not able to transition from open loop to FOC and runs into the startup failure error. I have increased my PWM frequency to 20kHz and the ramp up phase has become smoother. 

My motor shuts down at the same time irrespective of speed or torque control mode.