Motor will stop after ramp p
[PN]: custom Board based on evspin32g4-dual
[VERSION]: 6.4.0
[Motor]: Xing2207 1800Kv
[CubeMx]:6.14.1
Hello,
I have a problem with getting my FOC BLDC motor to start, the specs of the motor are: 0,08Ohm 50uH 0,32Vrms/kRPM. My project is for two sensorless motors with one shunt each, but I am trying to get started with the one connected directly to the stspin32G4.
When using 10kHz Pwm the motor first vibrates but does not spin, then it starts accelerating, then I get the startup failure. The failure always occurs when it reaches the start-up speed threshold. When I try 40kHz PWM it wont start at all. I noticed that in cubeMX there are some errors.
The schematic for the mosfet drivers is identical to the evspin32g4-dual:
33Ohm gate resistors and 1uF Boot Cap
I set the Boot charge time to 50ms and the Charging Duty cycle to 15%

Below is a screenshot of the startup phase once the motor is running, orange: one phase, blue: voltage over shunt, the digital signals are the gates of all three phases. Why are the phases not shifted 120 degrees?

How do I align the motor at startup, as I cant find the option?
Are those errors in CubeMx (picture below) critical?

Thanks for your help!!!!