Question
Motor wont start
- June 26, 2025
- 2 replies
- 442 views
Hello, I have a custom board based on the EVSPING4 Dual, the schematic is the same with the difference being no speed sensors and different mosfets. When I try to start the motor with motorpilot the speed is climbing in Motor Pilot but the motor is not spinning, after some seconds I get the error Start Up Failure. Motor Voltage and Voltage for the Gate Drivers are 12V. I measured the Phases of the motor and the Gates of the mosfets. The Phases are all on 12V as are the Gates of the top Bridge side. I added my schematic down below.