My Problem: My motor only runs when its max current is set to much less than its actual max current rating.
Hi, I have a 14-pole outrunner that's rated for 30A, but I get an overcurrent error every time. That changed when I tried changing its max current from 30A to 5A.
I still get two problems: 1) the motor never snaps to set speed, only oscillates about it; 2) when I load the rotor, I get a speed feedback error--I want the motor to increase torque to match the new torque demand when I apply a load to the rotor. This last point is my most important requirement.
I'll add that since auto-calculation of Kp and Ki for speed control is turned on, I'm wondering if it's worth trying to tune my motor parameters (Rs and Ls)? Using a motor config wizard from VESC, I obtained different values. I multiply them by 2 because I believe VESC gives phase resistance and inductance while ST Profiler gives line resistance and inductance. This new number gives something convincing.