No FreeRTOS for 6-step with kit P-NUCLEO-IHM03?
Hi there,
I am new to motor control and I am trying to set up my P-Nucleo-IHM03 kit with MC Workbench 6.1.2. I would like to use FreeRTOS in combination with the 6-step algorithm but in the "Application Configuration" under "FreeRTOS" it is stated: "Selected hardware boards do not support this feature".
I was wondering why FreeRTOS is not supported in this case?
With the *same hardware* and the FOC algorithm selected there is no such statement and I am having no issues generating a FreeRTOS project. So for 6-step I would now try to add FreeRTOS in STM32CubeMX, but I would like to know if there is any adamant obstacle that would prevent the combination of 6-step with FreeRTOS either in hardware or the 6-step library?
Thanks