Skip to main content
DHemb.1
Associate II
May 8, 2023
Solved

No USB enumeration of STEVAL-SPIN3201

  • May 8, 2023
  • 1 reply
  • 811 views

I am attempting to use an STEVAL-SPIN3201 eval board for the first time but cannot get it to enumerated on USB. LD2 flashes slowly indicating the embedded ST-LINK is operating. I have tried installing the Windows driver using en.stsw-link009, but no success. I've tried a variety of USB cables directly into the PC's USB port, as well as powering the board via J2. Windows (10) doesn't even blink when I plug the board in. Help is appreciated.

This topic has been closed for replies.
Best answer by DHemb.1

Well, as it turns out, though I tried several cables, the ones I tried were NOT compatible with the board to achieve communication with the USB port. I ordered a stand-alone ST_LINK/V2 programmer and tried the cable it came with and was able to enumerate the STEVLA-SPIN3201. Insert face palm here.

1 reply

DHemb.1
DHemb.1AuthorBest answer
Associate II
May 15, 2023

Well, as it turns out, though I tried several cables, the ones I tried were NOT compatible with the board to achieve communication with the USB port. I ordered a stand-alone ST_LINK/V2 programmer and tried the cable it came with and was able to enumerate the STEVLA-SPIN3201. Insert face palm here.