not enough torque
- December 31, 2025
- 4 replies
- 907 views
Good morning , I'm writing this post to request help , the main problem is two things the first and the main thing being the 1000W 3500 RPM 3 pole pair 48V motor not giving it rated torque of 2.5 Nm and only gives 0.8 N.m , this was confirmed as the motor works fine with a premade controller of the motor , further more the motor gets stuck and the torque reference goes to 19.99A however this does not happen with the premade controller , the motor works fine with the stm controller when no load is applied, the motor has been already profiled using the smt32 motor profiler, and motor barely gave any errors on the stm32 software however almost minimal torque, also as we are using a data acquistion system that is extremly accurate it measure 2A DC from the battery of 48V however the stm32 motor control software's torque reference showed 8.6 A , and the hall sensors are slight off , so at 370 RPM in the stm software its actually 500 and at 740 is 1000 and at 1110 its 1500 and soo on.
the reason we are trying to use the stm32 motor control software is to increase the efficiency
the motor is MY1020 BLDC, is hard to find its datasheet , our is silver color if it helps, take 3 pole pairs with grain of salt even thou we made sure it was 3.