Skip to main content
SDall
Associate III
February 10, 2022
Question

Odrive motor

  • February 10, 2022
  • 23 replies
  • 5489 views

hi i'm using a F401RE and a hmi016m1, using a brushless odrive motor, i'm using sdk notor control, i set motor type bull ranning, i left everything default the rest, but when i go to give the motor.start, the motor doesn't moves but makes a strange noise! what can i change?

This topic has been closed for replies.

23 replies

SDall
SDallAuthor
Associate III
February 10, 2022

it should be noted that the phase lights come on

GMA
Technical Moderator
February 10, 2022

Hello,

As far as I understood, you used "bull running" motor setting with your "odrive" motor test.

If yes, could you please use the "ST Motor profiler" tool in order to have the accurate motor parameters for your setup?

Best regards.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
SDall
SDallAuthor
Associate III
February 10, 2022

thanks I tried with this application but I can't connect with the serial I don't really know the reason, there must be something in the configuration for which the motor doesn't run but just makes a noise!

GMA
Technical Moderator
February 11, 2022

Ok, then did you modify the motor parameters in order to align them with the one you are using?

0693W00000JPQ2OQAX.png

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
SDall
SDallAuthor
Associate III
February 11, 2022

no the engine parameters I have not changed them, I left them by default! maybe they are the ones to change?

SDall
SDallAuthor
Associate III
February 11, 2022
GMA
Technical Moderator
February 11, 2022

According to this Odrive document, the Phase resistance is 0.039ohm, BullRun has 0.11ohm e.g.

I didn't check carefully, but Inductance seems to be missing in the document...

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
SDall
SDallAuthor
Associate III
February 12, 2022

I tried to change the resistor parameters 0.039, but it keeps giving me the same problem ......

SDall
SDallAuthor
Associate III
February 13, 2022

other thing i noticed that this engine is not surface psms but it is internal psms!

GMA
Technical Moderator
February 14, 2022

The magnetic structure could be modified in the Motor parameter box, but other parameters like inductance are missing from your documentation... This is why, you have to use the profiler first...

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA