Over Current Fault while I start to control the motor
Dear all,
I always encounter a "Over Current" fault once I click the "Start" button.

I have traced my phsae current by current probe, but it is shows less than 1A.

I have no idea what problems it is, has anyone can resolve it?
I list my platform and configuration as follows:
1. Motor Control Workbench 6.3.0
2. CubeIDE: 1.15.1
3. Control Board:NUCLEO-H563ZI
4. Power Board:X-NUCLEO-IHM08M1
5. Motor: SPMSM, 40V, 12A with an Encoder, 4096 cnts per revolution
Also, I have modified the HW configuration base on document description and workbench description


The other workbench configuration is listed as follow: