Over Current SW Fault with HSO [High Sensitivity Observer (Sensorless)]
- January 16, 2026
- 3 replies
- 407 views
Hi,
Currently I am evaluating HSO [High Sensitivity Observer (Sensorless)] in our custom Inverter board () with B-MOTOR-PMSMA1 motor. But when I start the motor it jerks and giving Over Current SW Fault.
Our custom board has following key components.
- Infineon 6ED2230S12TXUMA1 gate driver
- MCS1806GS-3-30-Z Current sensor





The same inverter board with B-MOTOR-PMSMA1 motor is working for Observer + PLL configuration.
I suspect that this board is having current sensor with ± 37.5 A measurement range designed for higher wattage motor giving fluctuation/slow response for B-MOTOR-PMSMA1 motor with 2.8A current rating.
Please help me to identify root cause of update project configuration to make it run with B-MOTOR-PMSMA1.
Attached following items for your reference.
- W30_SLIM_EVKMotor_HSO.stwb6 [MC Workbench config file]
- W30_SLIM_305_3IC_v4.json [HSO Inverter Board Designed File]
- W30_SLIM_305_3IC_v2.json [PLL Inverter Board Designer File]
- W30_SLIM_EVKMotor_PLL.stwb6 [PLL MC Workbench Config File]
Our end goal is to run Higher watt motor with our custom board. But first we need to understand HSO before and its tuning with smaller motor.