Over-Voltage Protection Options - Motor Braking Resistor Output No Longer Available In MC Workbench
Hi,
I am developing on EVSPIN32G4, MC Workbench 6.1.2.
The only option for Over Voltage Protection is to turn on Low Side Switches. This unfortunately doesn't work as I still constantly get Over Voltage faults in position control mode, when the motor is trying to stop on position. It generates enough back current to spike it above the threshold of 32V on a 24V PSU.
I have an older custom design with a large Braking Resistor switched by a MOSFET. The output for this option was available in earlier versions but I can no longer find it anywhere.
Are there any working solutions out of the box for over voltage protection?