Overcurrent Error When Applying Motor Parameters from P-NUCLEO-IHM03 to EVSPIN32G4-DUAL
After obtaining the motor configuration parameters using the P-NUCLEO-IHM03, I applied the same motor parameter values to the EVSPIN32G4-DUAL board, which is used to drive two motors.
However, when operating the motors with these settings on the EVSPIN32G4-DUAL, an overcurrent error occurs.
Could you please explain the possible reasons for this overcurrent condition?
In particular, I would like to know whether differences in the power stage, current sensing topology, or dual-motor operation could cause this issue, even when the same motor parameters are used.
Thank you for your support.
Best regards,
Pelino