Skip to main content
Associate II
March 22, 2024
Question

P-NUCLEO-IHM03 can't works

  • March 22, 2024
  • 3 replies
  • 2111 views

Hi st team,

I have purchase the P-NUCLEO-IHM03  development kit, i am using the development as the follows:

1, MotorControl workbench 6.2.1

2, STM32CubeMx 6.10.0

3, STM32CubeIDE1.14.1

 

I have try the follow steps:

1,In MotorControl workbench 6.2.1 i follow the example:

swingboard_0-1711086435395.png

without any change, i run it to generate project.

2, In STM32CubeMx to generate the code

3, In STM32CubeIDE1.14.1, compile it successful and run it to P-NUCLEO-IHM03

4, refer to "um2415-getting-started-with-the-xnucleoihm16m1-threephase-brushless-motor-driver-board-based-on-stspin830-for-stm32-nucleo-stmicroelectronics", i run the 'blue' button, the motor not running

 

so, would you give me any supports?

 

or give me a golden image for test in my P-NUCLEO-IHM03 kits to verify the hardware is all right?

    This topic has been closed for replies.

    3 replies

    GMA
    Technical Moderator
    March 22, 2024

    Dear @swingboard 

    Please have a look to this video presentation.

    If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
    Visitor II
    March 23, 2024

    i have follow the  steps on video, but it can't help me.

    any golden binary for me to test if the develop kit is ok in hardware?

    Visitor II
    March 23, 2024

    the kit's default setting  is for foc control way, your is introduce the '6-step' way.

    what about the golden foc binary?

    GMA
    Technical Moderator
    March 25, 2024

    Hello,

    You can use the "ST Motor Control Pilot" tool to connect the board and check internal board status.

    If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
    Associate II
    March 26, 2024

    it report "startup" error or "speed feedback" error.

    i have tried the st workbench 6.2.1  and st workbench 5.4.8, follow the "Speed ramp with Potentiometer on P-NUCLEO-IHM03 kit" example, both not works in my development kit.

     

    1, firstly to check if my development kit is wrong in hardware, can you give advice for it or give me the hex file in yourside?@GMA.

    2, i give you the hex file compiled in my side, can you try it in your board?@GMA

    Associate II
    March 26, 2024

    the hex/bin/elf file in my side

    GMA
    Technical Moderator
    March 29, 2024

    Hello @swingboard,

    For the motor, check that it spins freely and with a multimeter, that you have ~10 Ohm between each phase.


     

    If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA