P-NUCLEO-IHM03 giving startup failure
The P-NUCLEO-IHM03 with type selected as "FOC" has the firmware pre-installed. After pushing Blue start/stop button, the motor starts but fails to continue.
In Motor pilot, it is showing that a fault is thrown (startup failure) and the motor shuts down. The P-NUCLEO-IHM03 Black button needs to be pressed to clear the fault, but the motor still does not continue to run upon Blue button start.
Control Board: NUCLEO-G431RB
Power Board: X-NUCLEO-IHM16M1
Motor: Gimbal GBM2804H-100T