Phase current sensing problems
I am measuring the phase current signal, in between i see sudden spikes and the motor halts. I am testing at 60V battery input. It is hall based system and FOC.

It is a custom board and i have not configured the motor pilot, 2 questions if you can answer it will be helpful
a. If i am reading the phase currents at the middle of the low side pwm then it shall be consistently reading the same value but why suddenly it reads invalid value i do not understand i mean the spike.
b. If it is low inductance value should i mandatorily switch at 20KHz at present i am doing at 15KHz. What best i can do to identify the root cause.
Please advise based on the inputs i can move forward.