Phases Voltage Sensing support MC Workbench STM32H755ZI
Hi,
Is the Phases Voltage Sensing already supported for STM32H7 MCU's?
[PN]: STM32H755ZIT3
[VERSION]: MCSDK 6.3.2
[TOOL]: MC Workbench + Board Designer
[DETAILS]:
I've noticed that with a custom board I created that there's a small error under the Project Hw & Info tab saying that the Phases VoltageSensing is not supported for the selected MCU. I also see this coming into the connectAlgo.log file:
ERROR - Inverter Board: Following feature not supported by MCU: PhaseVoltageSensing
ERROR - Inverter Board: Following feature not supported by MCU: PhaseVoltageSensing

This error seems to disable the HSO mode for theSpeed Sensing Selection although the feature is available on the inverter board:

[EXPECTED BEHAVIOR]: When the feature PhasesVoltageSensing is configured for an inverter board/MCU the HSO should become available for Speed Sensing Selection in the MC Workbench .
[HOW TO REPRODUCE]:
- Configure an inverter with STM32H755ZIx MCU and add the PhasesVoltageSensing feature under the motor feature.
- Use the inverted in a workbench project
- See the error message under Project Hw & Info tab.
What does "not supported" mean in detail, what functions or configuration would be necessary to enable this for the H7 MCU?