Skip to main content
Associate
December 21, 2023
Question

PI控制调参

  • December 21, 2023
  • 2 replies
  • 848 views

sunboy_351_0-1703141662729.png

sunboy_351_1-1703141714429.pngMCSDK5.4.8版本 相最大电流270A,采样电阻0.0009欧,Lq 0.0991mH,Ld 0.04115mH,定子电阻0.01974毫欧,三电阻采样,相电流采样放大倍数3,电机相移角295度,PWM  16000Hz, 扭矩环调参后电机轴抱死,无法启动。

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    December 21, 2023

    Hello @sunboy_351 

    Correct me if this translation is incorrect.
    > The MCSDK5.4.8 version has a maximum current of 270A, a sampling resistance of 0.0009 ohms, Lq of 0.0991mH, Ld of 0.04115mH, a stator resistance of 0.01974 milliohms, three-resistor sampling, a phase current amplification factor of 3, a motor phase shift angle of 295 degrees, and a PWM frequency of 16000Hz.

    After adjusting the torque loop parameters, the motor shaft is locked and cannot be started.

     

    Have you tried reducing the gains? Have you tried X-CUBE-MCSDK-6?

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
    Associate
    December 22, 2023

    BMS128-60H  Motor(Hall)

     

    示例

    参数值

     

    示例

    参数值

    voltage platform

     

    60V/72VDC

    rated power

     

    1.5kW

    peak power

     

    4KW

    rated torque

     

    4.1N.m

    Peak torque

     

    45N.m

    peak current

     

    270A(45Nm)

    Max.speed

     

    5400rpm

    Ke

     

    8.63V/krpm(线反电动势有效值)

    POLE_PAIR_NUM

     

    3

    Lq

     

    0.09991mH

    ld

     

    0.04115mH

    Rs(line)

     

    19.74mΩ

    Max.fwcurrent

     

    212ARMS

    温度传感器型号

     

    MF58-503F3950

    Max.power

     

    4kW

    Max.torque

     

    45Nm

     

     

     

     

     

     

     

     

     

    rotational inertia

     

    2.6g.m2

     

     

     

     

     

     

    Motor parameter

    Workbench:

    sunboy_351_0-1703213299593.png

     

     

    sunboy_351_2-1703213335038.png

     

    sunboy_351_3-1703213357808.png

    sunboy_351_4-1703213371086.png

    sunboy_351_5-1703213386400.png

    test

    sunboy_351_6-1703213404268.png

    1 first start  status  under voltage

     

    sunboy_351_7-1703213497669.png

    sunboy_351_8-1703213511163.png

    2.clear  the  fault  next  start  

    motor Vibration  status  Run  is not faults

    sunboy_351_9-1703213657002.png

    Stop-> next start:  motor is not rotate

    sunboy_351_10-1703213688485.png

     

    Open loop   motor Normal rotation

    sunboy_351_11-1703214064385.png

    I use STM32F103RBT6, 64MHz, the above problem occurs, how to find the problem point?