problem about usage of steval-esc002v1
I succeeded in attaching steval-esc002v1 to the px4 system.
However, there is a problem that the motor is not smoothly controlled through the controller. If you look at the video, it looks like it's moving by step. Can you tell me what parameters I need to see?
At px4, the control pwm output is 400hz, and it has 36% IDLE duty and 43% ARMING duty. So STEVAL-ESC002V1.h is changed as follows
#define BSP_BOARD_IF_TIMx_MIN2MAX_BITS (11)
#define BSP_BOARD_IF_TIMx_MIN_SPEED_TON_US (1070)
In addition, since it is a no-load motor for quadcopter, MC_SixStep_param_7PP_3S_propeller.h was changed as follows
#define TARGET_SPEED 50000
Other parameters are the default provided in STSW-ESC002V1.