Reset issue STSPIN32F0A
Hello,
I have some troubles with the STSPIN32F0A when the load on the motor increases,
the STSPIN will reset.
The reset cause is checked in firmware at startup, and the cause mentioned is RCC_FLAG_PINRST.
Apart from a pull-up and a capacitor to ground, there is no hardware on the reset pin.
The voltage on the VDDA, VDD and VREG pin are correct at the time of reset.
What could be the cause of this reset?
Thanks.
Joris